Open a project
Open projects from a local folder, a network share, or a source repository.
- From the main menu, selectOpen.
- InSelect the project store file to open,navigate to the location of the project file.
- Select the project (.optix) file.
- SelectOpen.
TIP:
If the project was created using a previous version FactoryTalk Optix Studio, the
Project Upgrade
dialog box opens and lists the components to be updated. Select Upgrade
to upgrade and open the project.Provide Feedback