Set up a project

Create the project to use in the tutorial, and get to know the user interface.
Step #1: Create the project
  1. Start
    FactoryTalk Optix Studio
  2. Select
    New
    . The project templates window opens.
  3. Select
    Main project
    . This project includes the typical elements useful to design an HMI application.
  4. Set the project name. For example,
    MyProject
    , and the path in which to create it.
  5. Select
    OK.
      The project is created in the set path, inside a folder with the same name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.