Configure panel types
Configure panel types to distribute interface elements over multiple pages in the application.
- InProject view, right-clickUIand select .
- Hover-overNewFolder1, select, and enterEditPages
- Right-clickPagesand select .Panel1 (type)appears underPages.
- Hover-overPanel1 (type), select, and enterEditPage.
- SetWidthto1060andHeightto500.
- SetLeft margin, andRight marginto10.
- Right-clickPagesand select four times.Page1 (type),Page2 (type),Page3 (type), andPage4 (type)are created. EachPage# (type)inherits its properties fromPage (type).TIP: Inheriting properties enables you to quickly make modifications to parent object types and create consistent user interfaces. For example, if you want to changePage1 (type),Page2 (type),Page3 (type), andPage4 (type)margins, edit the margin properties ofPage (type). The modification will propagate to eachPage# (type).
Provide Feedback