- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Alarm grid
Use the
Alarm grid
widget to display and manage alarms at runtime. The Alarm grid
widget allows you to display and manage the alarms at runtime. View alarm information and acknowledge and confirm the alarms.Each row in the grid indicates a change in alarm status. Acknowledge and confirm one or all alarms on the grid. The
Alarm grid
widget displays these columns of information:
Column | Description |
---|---|
Timestamp | Date and time of the last alarm event update. |
Name | Name of the alarm object that generated the alarm event. |
Source variable | Variable the event monitors. |
Message | Message associated with the alarm event. |
Active | Whether the alarm is:
![]() ![]() |
Acknowledged | Whether the alarm is acknowledged or unacknowledged:
![]() ![]() |
Confirmed | Whether the alarm is confirmed or unconfirmed:
![]() ![]() |
Severity | Level of alarm severity from 1 to 1000. |
The
Alarm log grid
widget displays alarm events recorded by the configured event logger, such as the Alarm History Grid
. Use the Alarm History Grid with filter
widget to filter logged data.You can customize the data that appears in the
Alarm grid
by adding additional properties to an alarm to create an alarm type. See Create an Alarm grid.Provide Feedback