Automatically confirm and acknowledge alarms

Automatically confirm and acknowledge alarms

Reduce the interaction required to manage alarms at runtime. Have the application confirm and acknowledge alarms automatically.
  1. In
    Project view
    , select the
    Alarm grid
    .
  2. In
    Properties
    , configure:
    • Auto confirm
      . Select
      True
      to confirm that the issues causing alarms are resolved at runtime automatically. The
      Alarm grid
      displays only active and unacknowledged alarms.
    • Auto acknowledge
      . Select
      True
      to acknowledge alarms at runtime automatically. The
      Alarm grid
      displays only unacknowledged alarms.
      TIP: To have the
      Alarm grid
      display only active alarms at runtime, in
      Properties
      for the grid, set both
      Auto confirm
      and
      Auto acknowledge
      to
      True
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.