Create a converter type
Create a converter type and then use it to transform values in advanced dynamic links.
- InProject view, right-clickConvertersand select .
- (optional) Next to the converter object, selectto rename the converter.Edit
- InPropertiesset the converter property values.
Use the converter type instance to transform values in advanced dynamic links. See Create a complex dynamic link.
Provide Feedback