String formatter

String formatter

Modify the formatting of one or more values according to a customizable rule.
TIP: Using the string formatter, you can, for example:
  • Add characters before or after a value, if the value of the source variable numeric.
  • Format and parameterize SQL queries to use in database objects
  • Link multiple strings together in a series
  • Apply formatting, such as decimal places or float rounding, to numbers

Properties

Property
Description
Format
The formatting rule for variable reference:
  • Index. An index number that identifies an input variable. For every {index} placeholder in the formatting rule, a new field that indicated the source appears.
  • Alignment. An integer that represents the number of characters of the source value formatted according to the rule.
  • Format. The formatting to be applied to input variables.
    The format placeholder accepts a subset of values required by the .NET framework notation for the
    String.Format
    method. Placeholders must use the syntax
    {index,alignment:format}
    .
    TIP:
    To format a path (for example,
    ns=5;%PROJECTDIR%/Logo.svg
    ), you can use:
    • {index,alignment:
      filepath
      }
      . Format a string as a file path.
      Example:
      C:\Users\
      UserName
      \AppData\Local\Rockwell Automation\FactoryTalk Optix\Emulator\Projects\
      ProjectName
      \ProjectFiles\Logo.svg
    • {index,alignment:
      uri
      }
      . Format a string as a URI.
      Example:
      file:///C:/Users/
      UserName
      /AppData/Local/Rockwell Automation/FactoryTalk Optix/Emulator/Projects/
      ProjectName
      /ProjectFiles/Logo.svg
Mode
The direction of the dynamic link:
  • Read from source node to the parent.
  • Write from the parent to the source node.
  • Read from the source node to the parent and write from the parent to the source node.

Source

One or more variables, identified by a placeholder with an index number in the following {index} format. The index number is progressive and it must be an integer greater than zero {0}.
TIP: Placeholders can appear in any order in the formatting rule. For example, the syntax "the minimum value of {3}, {0} and {2} is {1}" is valid.

Data types

Example data: 23/04/2021 17:25:31, session with 60 minutes TimeZone offset.
DateTime
Format
Description
Example
g
Short date and time, local
  • (en-US): 4/23/21, 06:25 PM
  • (it-IT): 23/04/21, 18:25
F
Extended date and time, local
  • (en-US): Apr 23, 2021, 6:25:31 PM
  • (it-IT): 23 apr 2021, 18:25:31
X
Short date and time, UTC
  • (en-US): 4/23/21, 4:25 PM (UTC)
  • (it-IT): 23/04/21, 16:25 (UTC)
x
Extended date and time, UTC
  • (en-US): Apr 23, 2021, 4:25:31 PM (UTC)
  • (it-IT): 23 apr 2021, 16:25:31 (UTC)
U
Complete Universal Date and Time, UTC
  • (en-US): April 23, 2021 4:25:31 PM GMT (UTC)
  • (it-IT): 23 aprile 2021 16:25:31 GMT (UTC)
p
Short date, local
  • (en-US): 4/23/21
  • (it-IT): 23/04/21
P
Extended date, local
  • (en-US): April 23, 2021
  • (it-IT): 23 apr 2021
d
Short date, UTC
  • (en-US): 4/23/21 (UTC)
  • (it-IT): 23/04/21 (UTC)
D
Extended date, UTC
  • (en-US): Apr 23, 2021 (UTC)
  • (it-IT): 23 apr 2021 (UTC)
t
Short time, local
  • (en-US): 6:25 PM
  • (it-IT): 18:25
T
Extended time, local
  • (en-US): 6:25:31 PM
  • (it-IT): 18:25:31
h
Short time, UTC
  • (en-US): 4:25 PM (UTC)
  • (it-IT): 16:25 (UTC)
H
Extended time, UTC
  • (en-US): 4:25:31 PM (UTC)
  • (it-IT): 16:25:31 (UTC)
Numeric (Double Float Int16 Int32 Int64 Integer UInt16 UInt32 UInt64 UInteger)
Format
Description
Example
d
Numerical, without thousands separator.
After the format placeholder, the number of decimal places is configured with an integer (without padding).
  • d
    : -1234 ► -1234
  • d
    : 5.618 ► 5618
  • d2
    : 1,234.239 ► 1234.24
n
Numerical, with thousands separator.
After the format placeholder, the number of decimal places is configured with an integer (without padding).
  • n1
    : -1234.23 ► -1,234.2
  • n2
    : 5804.236 ► 5,804.24
  • n3
    : -1234.23 ► -1,234.2
e
Exponential notation.
After the format placeholder, the number of significant numbers is configured with an integer.
  • e10
    : 12345.6789 ► 1.234567890E4
  • e2
    : 2665.778 ► 2.7E3
f
Fixed point notation.
After the format placeholder, the exact number of decimal places is configured with an integer.
  • f3
    : 123 ► 123.000000
  • f3
    : 123.23 ► 123.230000
  • f4
    : -1898300.678 ► -1,898,300.6780
  • f3
    : 123.4 ► 123.400
p
Percentage.
After the format placeholder, an integer is used to configure the number of decimal places.
  • p
    : 1 ► 100%
  • p3
    : -0.397481 ► -39.748%
x
Hexadecimal notation.
255 ► ff
b
Binary notation.
107 ► 1101011
o
Octal notation.
56 ► 70
Duration and Timespan
Format
Description
Example
c
Constant format:
[-][d’.’]hh’:’mm’:’ss[‘.’fffffff]
  • 3.17:25:30.5000000
  • 4:30:00 AM
g
General short format:
[-][d’.’]hh’:’mm’:’ss[‘.’fffffff]
  • (en-US): 1:3:16:50.5
  • (en-US): 5:15:09:00
  • (fr-FR): 2:9:02:00,0200000
  • (fr-FR): 15:12:20:00
  • (en-US): 5:12:00
  • (fr-FR): 20:10:00
G
Extended general format:
[-][d’.’]hh’:’mm’:’ss[‘.’fffffff]
  • (en-US): 12:08:30 AM:00.0000000
  • (fr-FR): 12:08:30 AM:00.0000000
  • (en-US): 12:18:20 AM:00.0000000
  • (fr-FR): 12:17:30 AM:00.0000000
String
Format
Description
Example
l
All lowercase.
grüßEN ► grüßen
u
All uppercase.
grüßEN ► GRÜSSEN
t
All first letters uppercase.
grüßEN ► GRÜSSEN
f
Case independent.
grüßEN ► grüssen
ANSI SQL
Format
Description
Example
sql_identifier
Formats a given
String
or
LocalizedText
as a table or column identifier.
-
sql_literal
Formats the value of a variable as an SQL literal value (
Number
,
String
,
date
,
time
, and so on).
-

Inverse formatting

The inverse formatting feature allows you to modify a formatted value at runtime to replace it with a new value that the application shows with the same formatting at runtime.
The inverse formatting feature requires the following settings to operate correctly:
  • The dynamic link
    Mode
    of the converter must be
    Read/Write
    .
  • The
    Format
    field must have only one placeholder or source. The placeholder can have a suffix and/or prefix and be set with a format string such as {0:n}.

Output

The string entered in the
Format
property, based on the formatting rules with values in place of the placeholder or placeholders.

Logical representation

Example of a logical conversion in the

SQL queries examples

Parameterize the name of the internal column with the condition:
SELECT * FROM Table1 WHERE {0:sql_identifier} > 5
Comparison with a data variable:
SELECT * FROM AlarmsDatalogger WHERE Time > {0:sql_literal}
Parameterize the
LIKE
operator:
SELECT * FROM AlarmsDatalogger WHERE Name LIKE '{0}'
Parameterize a part of a query with a placeholder:
SELECT * FROM Table1 {0}
The placeholder with index
0
is linked to a project string variable and parameterizes a column; The placeholder with index
1
is linked to a numeric variable that represents the value for the comparison operator
>
:
SELECT * FROM {0:sql_identifier} WHERE Column1 > {1:sql_literal}
Parameterize the table name, the column and also the
LIKE
operator:
SELECT {0:sql_identifier} FROM {1:sql_identifier} WHERE {0:sql_identifier} LIKE '{2}'
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.