Remove a client device

Remove a client device

Remove client devices that you no longer need.
  1. From the main toolbar, next to
    Run
    Run
    , select the target client device drop-down.
  2. (optional) In
    Client device settings
    , to display only the active remote client devices, toggle Active remote devices.
    TIP: Refresh remote client devices by selecting Refresh.
  3. Select a client device.
  4. Select Remove the selected target device.
  5. In the
    Client device settings
    , select
    Remove
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal