Create a dynamic link by selecting the source

Create a dynamic link by selecting the source

Create a dynamic link using the
Properties
pane.
  1. In
    Project view
    , select the node that contains the property to set through a dynamic link.
  2. In
    Properties
    next to the property value to set, select  Add Dynamic Link.
  3. In the
    Dynamic Links
    browser, select a node to act as the source of the value property.
  4. (optional) To select a node attribute as the source, in
    Attribute
    , select an attribute.
    For example, select
    BrowseName
    ,
    Value
    , or
    DisplayName
    .
  5. (optional) If you select an array variable as the source, in
    Array Index
    , enter the index value of the variable to use.
  6. Click
    Select
    .
The reference to the selected node or variable appears in the property. For more information, see References to dynamic link sources.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.