Allow interaction with a graphic object

Allow interaction with a graphic object

Enable a graphic object so that users can interact with the object at runtime. Enable a graphic object in
Properties
.
  1. In
    Project view
    or in the window, select the container or graphic object.
  2. In
    Properties
    , in
    Enabled
    , select either:
    • True
      . The graphic object allows user interaction at runtime.
    • False
      . The graphic object prevents user interaction at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.