- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Delete a graphic object
Delete a graphic object to remove the object from the project. Delete a graphic object from either
Project view
or in the window.- InProject viewor in the window, select the container or graphic object and pressDelete.
The object is removed from the project.
Provide Feedback