Prevent changes to a graphic object

Prevent changes to a graphic object

Lock a graphic object to prevent changes to the object. Unlock an object to allowed continued changes.
  • In
    Project view
    or in the window, mouse over the container and select either:
    • Lock
      . The icon changes to and the graphic object is locked.
    • Unlock
      . The icon changes to and the graphic object is unlocked.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.