Rename a graphic object

Rename a graphic object

Rename a graphic object to give it a unique name. Rename a graphic object after adding an instance of or copying the object.
  1. In the window or
    Project view
    , select the graphic object.
  2. In
    Properties
    , in
    Name
    , select the name or select  and then type the new name of the graphic object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal