- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Apply animations to graphic objects
Add and configure number, sequential, or parallel animation properties to animate a graphic object.
- InProject view, select the graphic object to animate.
- InProperties, at the top, selectand then select either:Add
- Number animation.
- Sequential animation.
- Parallel animation.
For more information, see Animations. - Configure animation properties. See Animation properties.
Provide Feedback