- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Draw a rectangle or square
Use the
Rectangle
tool to draw rectangles or squares.- FromProject view, open the window to contain the object.
- In the editor toolbar, selectRectangle.
- In the window, position the crosshair where the square or rectangle is to begin.
- Drag to draw a rectangle or square.
The object appears in the window and in
Project view
.Provide Feedback