- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Draw an oval or circle
Use the
Ellipse
tool to draw and oval or circle.- FromProject view, open the window to contain the object.
- In the editor toolbar, selectEllipse.
- In the window, position the crosshair where the oval or circle is to begin.
- Drag to draw the oval or circle.
The object appears in the window and in
Project view
.Provide Feedback