Align graphic objects

Align graphic objects

Align selected items vertically or horizontally in the Design Area. Aligning objects increases and decreases the margins of the selected items.
  1. In
    Project view
    , double-click a container or select . The User Interface Editor opens.
  2. In the editor, select the graphic objects to align. To select multiple objects, hold down
    Ctrl
    and select additional items.
  3. In the Design Area toolbar, select the icon to align the selected graphic objects in the Design Area:
    •   Align at the left border.
    •   Aligns at the top border.
    •  Align at the right border.
    •   Align at the bottom border.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal