Move a graphic object
Move a graphic object in the window to position objects as they will appear at runtime. All of the objects in a container move with the container.
- To move a graphic object either:
- In the window, select and drag the container or graphic object.
- InProject view, select the container or graphic object and then inPropertieschange:
- Horizontal alignment. Enter the value for the space between the object and the x-axis.
- Vertical alignment.Enter the value for the space between the object and the y-axis.
TIP: The order of graphic objects on the z-axis compared to other objects in the same container is determined by the position of the graphic object inProjectview. Objects lower in the tree appear higher in the order on the z-axis.
Provide Feedback