Select a style sheet

Select a style sheet

Select the style sheet for a
FactoryTalk Optix Application
to display at runtime.
TIP: You can edit the global and style controls to edit either the styles of all objects in the project, or just the styles of specific object classes.
  1. In
    Project view
    , select the
    NativePresentationEngine
    engine object.
  2. In
    Properties
    after
    Style sheet
    , select the drop-down arrow after the style sheet value and select the style sheet for the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.