- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Communicate with Azure IoT Hub broker
Azure IoT Hub supports sending or receiving information only on specific topics of a device.
Azure IoT Hub does not allow to send and receive information on custom topics. A device can send or receive information only on specific topics of the device:
- send
- devices/deviceid/messages/event/
- receive
- devices/deviceid/messages/devicebound/#
- For each client that to send or receive messages, create a device on Azure IoT Hub.TIP: Clients cannot use the same devices to send or receive data.
- Verify that sending and receiving messages is successful.TIP: The Device Explorer and Azure IoT Explorer applications enable you to monitor the received messages and send messages to devices.
Provide Feedback