Create a library folder

Create a library folder

Create a folder in a local or remote library to organize the templates that belong to that library.
  1. From the main toolbar, select
    Template Libraries
    Template Libraries
    .
  2. Select a library in which you want to add a folder.
  3. In
    Template Libraries
    , select
    Add
    Add
    and select
    New folder
    .
  4. (optional) Enter a name for the folder.
New folder appears under the selected library in
Template Libraries
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal