Create a remote library

Create a remote library

Create a custom remote library to store templates of objects and variables.
  1. From the main toolbar, select
    Template Libraries
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Add
    Add
    and select
    New remote library
    .
  3. In
    Remote location
    , enter a URL to a Git repository to store the library.
    IMPORTANT: Ensure that the Git repository is safe to store the remote library. Contact a repository administrator to learn who can access the repository.
  4. (optional) Enter a name for the library.
New local library appears in
Template Libraries
.
Add templates to your library. See Create a template from an object or variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal