- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Add a locale language to a localization dictionary
Add locale languages to a localization dictionary so you can change the language displayed for an application at runtime.
- InProject view, expandTranslationsand double-click a localization dictionary.
- In the localization dictionary, in theTranslation tableview, selectAdd locale.
- UnderSelect the new locale, select a locale language and then select
.
- InNew locales added, to add the locale to the displayed objects, selectYes.
A new column appears for the locale.
Provide Feedback