Open an object
Open an object from
Project
view
. - InProject view, double-click the object or mouse over the object and then select
.
The object opens if the object has a dedicated editor.
Properties
for the object open.Provide Feedback