Add limits to a variable

Add limits to a variable

Add minimum and maximum limits to numeric variables. Limits impose certain behaviors when the value is outside of the limits.
  1. In
    Project
    view
    , select the variable.
  2. In
    Properties
    , right-click the numerical variable and select
    New >
    Range
    .
  3. Under
    EURange
    , complete:
    • Low
      limit
      . Enter the low limit for the value of the variable.
    • High
      limit
      . Enter the upper limit for the value of the variable.
    • Constrain
      . Set to true to constrain the values for the variable for the low and high limits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.