Change the unit of measure for a variable

Change the unit of measure for a variable

Change the unit of measure for a variable that displays at runtime.
  1. In
    Project view
    , select the variable.
  2. In
    Properties
    , select the unit of measurement in the value of the variable.
  3. In the
    EUInformation Editor
    , select the unit of measure and choose
    Select
    .
The new unit of measure appears in the value for the variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.