- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Remove a unit of measure from a variable
Remove the unit of measure for a variable to no longer have the value for that variable appear in that unit of measure.
- InProjectview, select the variable.
- InProperties, in the value for the variable, select the unit of measure.
- In theEUInformation Editor, select the unit of measure and selectDelete.
- SelectOK.
The unit of measure is removed from the variable.
Provide Feedback