Set the unit of measure for a variable
Set the unit of measurement for a numeric figure.
- InProjectview, select the variable.
- InProperties, right-click the numeric value and selectNew > EUInformation.
- In theEUInformationEditor, select the unit of measure for the variable and chooseSelect.
The unit of measure appears in the value for the variable.
Provide Feedback