Import Companion Specifications
Add support for more Companion Specifications to
FactoryTalk Optix Studio
.Prerequisites
- Obtain anXMLfile with Companion Specifications to import.
- CloseFactoryTalk Optix Studio
- To import Companion Specifications
- Copy theXMLfile with Companion Specifications toC:\Program Files\Rockwell Automation\FactoryTalk Optix\Studio\CompanionSpecifications
- If prompted, selectContinue.
The imported Companion Specifications are available in
FactoryTalk Optix Studio
.Provide Feedback