Configure the trusted certificates at runtime

Configure the trusted certificates at runtime

Configure a server or client certificate rejected at runtime as a trusted certificate.
You can move the certificate in the following ways:
  • Manually, by using Windows Explorer (only on Windows target).
  • Remotely, by using FactoryTalk Remote Access.
  • By using the same application.
  • From
    ApplicationFiles/PKI/Rejected
    , move the certificate to
    ProjectFiles/PKI/Trusted/Certs
    .
After a few seconds, the certificate is considered trusted without the need to restart the
FTOptixApplications
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.