Configure the trusted server certificates at design time

Configure the trusted server certificates at design time

Set the server certificate rejected when importing nodes with an OPC UA client object as trusted to be able to import these nodes at design time.
You can move the certificate in the following ways:
  • Manually, by using Windows Explorer (only on Windows target).
  • Remotely, by using FactoryTalk Remote Access.
  • By using the same application.
  • From
    ApplicationFiles/PKI/Rejected
    , move the certificate to
    ProjectFiles/PKI/Trusted/Certs
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.