- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Add an OPC UA client object
Configure an OPC UA (OPC Unified Architecture) client by adding an OPC UA client object to the project and configuring its properties.
- InProject view, right-clickOPC-UAand select .
- InProperties, set the OPC UA client object properties.For more information on the properties, see Object and variable references.
Provide Feedback