Configure firewall for an OPC UA server

Configure firewall for an OPC UA server

If an application has an OPC UA server running in Windows®, open the port specified in the
Endpoint URL Server
property of the OPC UA server.
  • When running a project with an OPC UA server object, if prompted, accept requests for configuring a firewall rule.
The
runtime
firewall rule is created.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.