- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Certificates and keys location
The certificates and keys are organized in this folder structure.
Certificates and keys in projects
ProjectFiles/PKI
- Own
- Certs. Allowed application certificates.
- Crl. Revoked application certificates.
- Trusted
- Certs. Allowed certificates of trusted remote applications.
- Crl. Revoked certificates of trusted remote applications.
- Issuers
- Certs. Allowed Certification Authority (CA) certificates.
- Crl. Revoked CA certificates.
Certificates and keys in runtime applications
ApplicationFiles/PKI
- Rejected. Rejected certificates of remote applications that are not trusted.
Provide Feedback