Configure a recipes editor widget

Configure a recipes editor widget

You add a recipes editor widget by selecting it from the template libraries and editing its properties.
TIP: You can develop your own recipes management solution. For more information, see Custom recipes management interface.
  1. From the
    FactoryTalk Optix Studio
    toolbar, select
    Template libraries
    .
  2. In :
    1. Select
      Widgets
      .
    2. Drag
      Recipes Editor
      to the
      UI
      folder in the
      FactoryTalk Optix Studio
      pane.
    3. Select
      Close
      .
  3. In the pane, double-click the
    RecipesEditor
    object.
    The widget preview displays in the central pane.
  4. In the pane, in the
    RecipeSchema
    property, select a
    Recipe Schema
    object.
  5. In the pane, automatically configure the graphical objects and dynamic links used to assign values to ingredients at runtime by right-clicking the
    RecipesEditor
    object and selecting
    Execute Setup
    .
The ingredients appear in the widget.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.