Configure idle timeout for a page

Configure idle timeout for a page

Use a NetLogic to configure an idle timeout if you want the timeout to apply only a specific page or panel. Idle timeouts configured using a NetLogic do not apply to the entire project.
  1. Select
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Scripts
    .
  3. Under
    Components
    , drag
    Idle Timeout
    directly into the start window, such as
    MainWindow (type)
    , in
    Project view
    .
  4. In
    Libraries
    , select
    Close
    .
  5. With
    IdleTimeoutLogic
    selected, in
    Properties
    , in
    Enabled,
    select
    True
    to enable NetLogic. Enabling
    IdleTimeoutLogic
    enables the timeout by default.
  6. In
    Duration
    , enter the time before the timeout occurs.
  7. In
    Project view
    , expand
    IdleTimoutLogic
    and then select
    OnTimeout
    .
  8. In
    Properties
    after
    OnTimeout
    , select .
  9. In the browser, expand
    Commands
    , expand the type of command, and then select the command that will be executed when the timeout event is triggered.
  10. Click
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.