- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Configure idle timeout for a session
Use the UI Session
IdleTimeoutEvent
to have an idle timeout apply to the entire session and the Presentation Engine.- InProject view, right-click theUIfolder and selectNew > UI Session.UISession# (type)appears inProject view.
- WithUISession# (type)selected, inProperties, inInactivity timeout duration, enter the duration for the timeout.
- InInactivity timeout active, selectTrue.
- UnderEventsafterIdleTimeoutEvent, selectAdd new method, expandCommands, and navigate to select the command that will be executed when the timeout event is triggered.
Provide Feedback