- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Customize standard units of measure
The session locale determines the measurement system for the displayed data. For example, a session with the en-US locale displays temperatures in Fahrenheit degrees.
Customize measurement units at the project level to use different measurement systems for each desired quantity. For example, import data from a sensor configured in a custom degrees format but display the value in Celsius at runtime. To customize units of measure, map the measurements in the
Measurement systems map
.- InProject view, select the project root node.
- InProperties, afterMeasurement systems map, selectEdit with Measurement system editor.
- In the title bar of theMeasurementSystemMapthat opens in the center of the screen, select
. A new row appears in the map table.
- In theFromcolumn, select the input quantity of interest or the value from the sensor. The selected units of measure will be translated to the equivalent quantity for the different locales in the three remaining columns.
- In theInternational System of Units,US Customary Measurement System, andBritish Imperial Units columns, select the desired target measurement units.
Provide Feedback