Create buttons to control alarms

Create buttons to acknowledge and confirm a selected alarm or all alarms.
  1. Create a button for acknowledging all alarms:
    1. In
      Project view
      , right-click
      AlarmGridPanel
      and select
      New
      Base controls
      Button
      .
    2. Hover-over the button, select
      Edit
      , and enter
      AcknowledgeAllButton
      .
    3. In
      Properties
      , set
      Text
      to
      Acknowledge All
      .
    4. In
      Events pane
      , next to
      MouseClick event
      , select
      Add
      and select
      Commands
      Alarm commands
      Acknowledge all
      .
  2. Create a button for confirming all alarms:
    1. In
      Project view
      , right-click
      AlarmGridPanel
      and select
      New
      Base controls
      Button
      .
    2. Hover-over the button, select
      Edit
      , and enter
      ConfirmAllButton
      .
    3. In
      Properties
      , set
      Text
      to
      Confirm All
      .
    4. In the
      Events pane
      , next to
      MouseClick event
      , select
      Add
      and select
      Commands
      Alarm commands
      Confirm all
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.