- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Integrate the interface with the NetLogic
Make the button trigger the label text change when you select the button.
- InProject view, selectButton1.
- InEvents, next toMouseClickEvent, selectand select .
- Create a dynamic link betweenlabelNodeIdandLabel1.For more information about dynamic links, see Create dynamic links.
Provide Feedback