- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create a NetLogic that generates random data
This script generates random data and populates the Store1 database tables with it.
Prerequisites
Set the default external code editor. See Set the default code editor.
- InProject view, right-click theStore1folder and select .
- Hover-over the NetLogic, select, and enterGenerateRandomData.
- Double-click the NetLogic.The external code editor opens.
- In the code editor, replace the existing code with the following code:using System; using FTOptix.Core; using Store = FTOptix.Store; public class GenerateRandomData: FTOptix.NetLogic.BaseNetLogic { public override void Start() { // Insert code to be executed when the user-defined logic is started } public override void Stop() { // Insert code to be executed when the user-defined logic is stopped } [FTOptix.NetLogic.ExportMethod] public void InsertRandomValues() { // Get the current project folder. var project = FTOptix.HMIProject.Project.Current; // Save the names of the columns of the table to an array string[] columns = { "Column1", "Column2", "Column3", "Column4" }; // Create and populate a matrix with values to insert into the odbc table var rawValues = new object[1000, 4]; Random randomNumber = new Random(); for (UInt16 i = 0; i < 1000; ++i) { // Column1 rawValues[i, 0] = i; // Column2 rawValues[i, 1] = randomNumber.Next(0, 5000); // Column3 rawValues[i, 2] = randomNumber.NextDouble() * 5000; // Column4 rawValues[i, 3] = Guid.NewGuid().ToString(); } var myStore = LogicObject.Owner as Store.Store; // Get Table1 from myStore var table1 = myStore.Tables.Get<Store.Table>("Table1"); // Insert values into table1 table1.Insert(columns, rawValues); } }
- Save the code.
Provide Feedback