- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create a database
You must add table to the data store before you start querying it.
- InProject view, right-clickDataStoresand selectEmbedded databaseorODBC database.
- InProperties, next toTablesselect.
- Add three table columns of Int16, Int32, and Float data types:
- Under the created table, next toColumnsselect.
- Next to the column, selectBaseDataTypeand selectInt16.
- Next toColumns, select.
- Next to the column, selectBaseDataTypeand selectInt32.
- Next toColumnsselect.
- Next to the column, selectBaseDataTypeand selectFloat.
Provide Feedback