Create a NetLogic that fetches panels

This NetLogic fetches a panel from the Server project and loads it in the Client project.
Prerequisites
Set the default external code editor. See Set the default code editor.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Runtime NetLogic
    .
  2. Hover-over the NetLogic, select
    Edit
    , and enter
    PanelFetcher
    .
  3. Double-click the NetLogic.
    The external code editor opens.
  4. In the code editor, replace the existing code with the following code:
    #region Using directives using System; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; using FTOptix.HMIProject; using FTOptix.Retentivity; using FTOptix.NativeUI; using FTOptix.UI; using FTOptix.OPCUAClient; using FTOptix.Core; using FTOptix.CoreBase; using FTOptix.NetLogic; using FTOptix.UI; #endregion public class PanelFetcher : BaseNetLogic { public override void Start() { var importedPanel = Project.Current.Get("UI/Panels/Panel1"); if (importedPanel == null) { Log.Error("Could not find remote panel"); return; } var mainWindowPanelLoader = LogicObject.Owner.Get<FTOptix.UI.PanelLoader>("ClientPanelLoader"); // Change panel to the imported remote panel. mainWindowPanelLoader.ChangePanel(importedPanel.NodeId, NodeId.Empty); } public override void Stop() { // Insert code to be executed when the user-defined logic is stopped } }
  5. Save the code.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.