Add users (server)
Create multilingual users.
Prerequisites
Add the it-IT locale. See Add a locale language to a localization dictionary.
- Create a folder for domain users:
- InProject view, expandSecurity.
- Right-click theUsersfolder and select .
- Hover-over the folder, select, and enterDomainUsers.
- Create the domain users:
- Create two users by right-clickingDomainUsersand selecting .
- Rename the users by hovering-over each user, selecting, and entering:
- Alice
- Frank
- InProject view, selectAlice.
- InProperties, setLocaleIdstoen-US.
- InProject view, selectFrank.
- InProperties, set theLocaleIdstoit-IT.
Provide Feedback