Develop a solution for importing UI

Use OPC UA communication to import the UI from another project and display the values of selected variables.
Application example (server and client)
TIP:
Download a sample project:
ImportUI.zip
Prerequisites
TIP: The Client project imports data from the Server project.
Application design example (server and client)
In
FactoryTalk Optix Studio
, select
Run
to run Server and Client projects using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.