- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create a button that closes the application
Create a button that closes the
FactoryTalk Optix Application
application.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enterCloseApplicationButton.
- InProperties, setTexttoClose application.
- InEvents, next toMouseClick event, selectand select .
Provide Feedback