Develop a user-specific interface

Develop a user-specific interface

Provide personalized user experience and make certain interface areas accessible only for particular user groups.
Application example
The
Admin Pane
is only visible for logged-in administrators.
NOTE:
Download a sample project:
UserSpecificInterface.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.