Develop an icon that changes color
Implement an image of a conveyor that changes the color of its chassis based on the associated alarm state.
NOTE:
Download a sample project:
ChangeIconColorBasedOnAlarm.zipApplication example - disabled alarm
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/ChangeIconBasedOnAlarm1.png/_jcr_content/renditions/original)
Application example - enabled alarm
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/ChangeIconBasedOnAlarm2.png/_jcr_content/renditions/original)
Prerequisites
- Download, extract, and copy the SVG 1.2 Tiny image into thefolder:ProjectName/ProjectFilesTIP:To enable the selective image color manipulation, the image part of interest must have a unique@idattribute assigned.For example:<gid="ConveyorChassis"> <polygon style="fill:#3C4660;" points="8.532,379.733 503.466,379.733 503.466,277.333 8.532,277.333"/> </g>
- To develop the project
- Arrange the interface elements.
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/ChangeIconBasedOnAlarmDesign.png/_jcr_content/renditions/original)
In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select Run
Provide Feedback