Implement the UIPopulator NetLogic

Implement the UIPopulator NetLogic

Point the NetLogic to the graphic objects.
  1. In
    Project view
    , select
    UIPopulator
    .
  2. In
    Properties
    , at the top, select
    Add
    and select
    Variable
    .
  3. Hover-over the variable, select
    Edit
    , and enter
    ModelObject
    .
  4. Next to
    ModelObject
    , select
    Int32
    and select
    NodeId
    .
    TIP: If you do not see the required option, select the
    Show all
    checkbox.
  5. Create a dynamic link between
    ModelObject
    and
    ProjectName
    UI
    MainWindow (type)
    ListBox1
    Selected item (Pointer)
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.