InformationModel.MakeAlias(browseName)

Creates an alias and returns a corresponding
IUAVariable
C# object.
static IUAVariable MakeAlias(QualifiedName
browseName
);

Arguments

browseName
(QualifiedName)
The
BrowseName
of the new alias.

Returns

IUAVariable
A C# object that corresponds to the project object created.

Example

The following example shows an alias that is created in the
Motor1
object of the
FactoryTalk Optix Studio
project:
var modelFolder = Project.Current.Get("Model"); var alias = InformationModel.MakeAlias("CurrentMotor"); modelFolder.Add(alias); modelFolder.SetAlias("Model", Project.Current.Find("Motor1"));
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.